12/14/2023 3:51 AM | |
Posts: 1 Rating:
|
Dear All, I'm trying to communicate LOGO 6ED1052-1MD08-0BA1 using Ethernet from the VB.NET code provided in this thread to cater my customer's requirement monitoring & reading the IO values. According to the product manual changed the Port from 10001 to 8443 in the .net code and tried to communicate PLC and able to Connect / Disconnect Successfully. Other Functions such as GetPLCStatus, Run / Stop PLC is not working, getting the error message "Error: Read Time Out. Detail Error Code : DTx0108L01". From the previous replies in this thread, amended the changes in the code as below: - increased the Send / Receive Timeout till 200000 ms, and encountering the same error. - Sync time between PC and PLC. - Enabled Allow S7 access, Allow Modbus access in the LOGO Comfort V8.3.0 Offline settings. Can I get some help in this...? Thanks in advance. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/14/2023 10:05:37New subject after splitting and Text formatting optimized |
|
Follow us on