6/18/2019 9:55 AM | |
Posts: 16 Rating:
|
I have a SIMOVERT MasterDrive Chassis Unit Installed on a site with is currently controlled by S7-200 PLC via USS communication (Scom2). The S7-200 PLC is getting old and i need to replace it with S7-1200 PLC. The Drive will remain the same. Now i have to implement the USS communication with the new S7-1200 but i am not able to find any Application Example for this exact scenario. I found example of S7-1200 with V20 Drive;https://support.industry.siemens.com/cs/ww/en/view/109480894 In this example, USS is implemented using SIMATIC S7-1200 CM1241 communication module (6ES7241-1CH32-0XB0) or SIMATIC S7-1200 CB1241 communication board (6ES7241-1CH30-1XB0) alternatively. Can this example be implemented with SIMOVERT USS communication using the specified S7-1200 Hardware in the above example.? |
Last edited by: Jen_Moderator at: 06/18/2019 13:57:59Optimized link. |
|
12/27/2023 3:02 PM | |
Joined: 8/21/2014 Last visit: 9/16/2025 Posts: 1087 Rating:
|
New question published by mestomes is split to a separate thread with the subject MasterDrive-Communiaction with S7-1200 through USS. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on