(0)| 1/30/2024 5:49 AM | |
|
Joined: 3/30/2020 Last visit: 12/11/2025 Posts: 5656 Rating:
|
For help on how to update the firmware, refer to point 6 in the following web page.. The formal information is available in the System Manual.. About the download site for the manual.. select the version you wish to use. The instruction for updating the firmware per memory card did not change between manual versions. See the comment from @0_Einstein to get hold of the firmware that should be loaded into the PLC. (The search facility within these support pages is your friend.) |
Last edited by: qwazee at: 01/30/2024 05:51:18Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on