(0)| 3/14/2024 2:02 PM | |
|
Joined: 4/16/2022 Last visit: 6/13/2025 Posts: 3 Rating:
|
Good morning Can anyone kindly help me? I have the PAC 3200 and 3220 in the industry and I also need to read the values "Total active energy Import Tariff 1", but I have already made several attempts and read several forums, but without success. I would like to know how I insert addresses into MB_Client and how to structure it. The other values such as voltage, current, power, I was able to read normally, my problem is in active energy tariff 1. Thank you very much in advance! ------------------------------------------------------------------------------------------ |
Last edited by: rafael.portugal at: 03/14/2024 14:02:53Last edited by: The Helping Hand at: 03/15/2024 12:48:27New subject after splitting and text formatting optimized |
|
Follow us on