3/21/2024 8:44 AM | |
Joined: 8/3/2009 Last visit: 9/10/2025 Posts: 16386 Rating:
|
Hello GTSAGarcia A Windows PC (and also the Simulation) uses another Syntax and Filesystem functions than on a Windows CE Panel. So you cannot use the same code in Simulation and on the real panel. For example here are some information about the two different systems: PC-based WinCE Panel The functions for WinCE are also explained in the Help System Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on