(0)| 5/10/2024 6:32 AM | |
|
Joined: 5/10/2024 Last visit: 6/26/2025 Posts: 1 Rating:
|
Hello guys, I am working on a project in Wincc Scada. Let me explain my situation to you. I have a button in HMI for changing mode of operation. I have assigned a bit tag to button. But I want to provide a confirmation window that pop ups when button is clicked to ask for permission to really change mode.. Regards Suy ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/10/2024 08:54:27New subject after splitting |
|
| 5/15/2024 11:02 AM | |
|
Joined: 8/3/2009 Last visit: 1/9/2026 Posts: 16629 Rating:
|
Hello First of all which WInCC do you use? there are a few option at the moment for a WinCC SCADA system... If you have WInCC V7/8/Professional you could use simply a messagebox with confimation buttons. https://learn.microsoft.com/de-de/office/vba/language/reference/user-interface-help/msgbox-function Its a simple and fast way. If you use a Touch Screen and the standard MsgBox does not work because of design and size then you would have to use an own WInCC workaround with Screen windows. In WinCC V8 there is also a possibility to use popup Screens Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on