5/24/2024 8:52 PM | |
Joined: 2/1/2010 Last visit: 9/16/2025 Posts: 213 Rating:
|
Without new function for 7.1 > 9.1 must mean you are on standard library - V7.1 SP3 Upd4 (non-APL). In this case, as long as you are on the version mentioned above, you can expect it to work the same in 9.1 as it did in 7.1 as long as you followed all the upgrade rules including dealing with the basis library as needed (which might include with new functionality). There will not be any issues compiling or working if all of it has been handled correctly and no other crazy libraries like you mentioned (common library issues being: simocode, modbus, asi, etc.) If you weren't already on standard library V7.1 SP3 Upd4 then you have to upgrade to that along the way.
If you are on any APL version (even if just 1 block mixed in) then you have to upgrade with new functionality for APL library and basis to get from 7.1 > 9.1 based on library compatibility matrix, in compat tool. Pick a compatible APL and basis version, which may or may not be the highest, based on if you are trying to standardize between multiple MPs. You can get a visualization of options with this article: |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to
1 thankful Users |
Follow us on