7/12/2024 1:52 PM | |
Joined: 7/10/2024 Last visit: 8/22/2025 Posts: 180 Rating:
|
Hello! Regardless of whether it is an ITP1000 or a PC, the way to configure the runtime advanced is the same. You will need to include a PC Station in the TIA Portal and insert both the WinCC RT Advanced component and the network card and make the HMI connection between the RT Advanced and the PLC. In this FAQ: https://support.industry.siemens.com/cs/af/en/view/89852595 you will find how to perform these steps. I hope it works |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on