(1)| 3/11/2008 4:14 PM | |
|
Joined: 9/29/2005 Last visit: 12/2/2025 Posts: 313 Rating:
|
Hi once again, i am sorry but i have no idea so far. What you wrote here is exactl what i would do regarding Hardware INterface description and AT command set. only a few stupid ideas: - changing button 1 with button 2 - Ensure that you close the pin 5 before configurate it --> AT^SCPIN=0,5 --> AT^SCPIN=1,5,0 - do a factory reset - What does this mean (Hardwaredescription TC65 Terminal Chapt. 3.5.5.): "The state of several pins will change again once the respective interface is activated or configurated by AT command" - Is your wiring ok regarding the GPIO connector? See picture 11 in the manual regards |
Last edited by: Lifrasil at: 11.03.2008 16:15 |
|
| 3/18/2008 9:20 AM | |
|
Posts: 10 Rating:
|
to jquim: Hex string in error is PLKMERR,5003:0c40:e010 Monaco: SPORTs: BSPORT Lockup I do not know meaning of error. to Lifrasil: I'm sorry but is seams that my prevoius post isn't posted well so I'll type it again. Problem with GPIO 5, 7 and 9 isn't in TC65. By (fourth) detail examination of board I noticed one more chip (some smd with 6 pins) that is connected to pins 5, 6, 7 and 9. So I'm sorry to wasting Your time and thanks again for new firmware that solved priblem with restart. Is it possible to somehow obtain a pdf (should be called) TC65_hd_v03000.pdf. It seams that startup states of pins after power are not the same on firmware ver 02.000 and 03.000. Regards, nedeljko |
Last edited by: ndivjak at: 3/18/2008 9:23 AM |
|
| 3/20/2008 11:50 AM | |
|
Posts: 10 Rating:
|
Finally I've got electric diagram of the board from my suplier. Pins GPIO6 and DAI0 are connected to the same board port pin 1, GPIO7 and DAI1 are connected to the same board port pin 2, GPIO8 and DAI2 are connected to the same board port pin 3 and GPIO10 and DAI3 are connected to the same board port pin 4. DAI0, DAI2 and DAI3 are output pins and DAI1 is input pin. That is reason that I got good behaving on GPIO7(software GPIO6) and on the other pins I allways got output from DAI pins and not from board port. Is it possible to convert pins DAI0, DAI1, DAI2 and DAI3 to high-impendace state by some AT command? |
| 4/15/2008 10:20 AM | |
|
Joined: 9/29/2005 Last visit: 12/2/2025 Posts: 313 Rating:
|
Dear TC65 User, maybe not really satisfying for you, but very satisfying for me because it increases the worth of this article i.m.h.o. Your failure (regarding EXIT...) where recognized and here is the answer from the support:
I will provide you with the most actual firmware when available. |
| 6/25/2009 11:20 AM | |
|
Posts: 1 Rating:
|
Hi, we're upgrading some module to Fw Rev 3.0. Do you have any news about the bugs on I/0s ? Do you know if there is e newest Fw relese since April 08 ? Thanks Massimo |
Follow us on