7/22/2024 5:15 PM | |
Posts: 2 Rating:
|
Hi, I am working on a pcs7 project V7.0 Sp1. We have a ES & a server and when download the project to the server via wincc , not able to choose only change But if I try to download the entire project, then its getting downloaded successfully. ------------------------------------------------------------------------------------------ |
Last edited by: Wit_Moderator at: 07/25/2024 07:24:11New subject after splitting |
|
7/31/2024 5:05 AM | |
Joined: 1/11/2019 Last visit: 8/14/2025 Posts: 899 Rating:
|
Hello, When changes are made on the OS machine, you may not be able to download only the changes. Here is the solution: Solution:
Note: DO NOT perform a full compilation if you intend to download only the changes. |
Follow us on