(0)| 8/9/2024 3:49 PM | |
|
Joined: 6/26/2016 Last visit: 2/4/2025 Posts: 4 Rating:
|
Hi, I'm having issues trying to get channel faults from the following devices on IM 153-4 PN racks: - 6ES7 331-7NF10-0AB0 / AI 8x16BIT - 6ES7 331-7PF01-0AB0 / AI 8xRTD I'm using SFC51 with SZL_ID = w#16#00B1 and getting error code 8083 which means the INDEX is incorrect or not permitted. The INDEX apparently should be the Logical Base Address of the module. As you can see from the photos attached this is 256 or 16#0100 for the module I'm trying to get the diagnostics from. Any help on this would be appreciated. Thanks Attachmentattachment.pdf (976 Downloads) |
Last edited by: AutoGen_412547 at: 08/10/2024 09:14:23Last edited by: Moderator_Lan at: 08/12/2024 07:53:42attachments combined to pdf |
|
Follow us on