(0)| 8/13/2024 5:32 AM | |
|
Joined: 9/11/2014 Last visit: 12/18/2025 Posts: 890 Rating:
|
Hi, I have used the attached program for testing with a LOGO! 8.4: I have set both bits to "1" in online test. Then I have done a power cycle at the LOGO! 8.4. Here the result after the power cycle and restart of the online test: VR0.0 has still "1" signal, V0.0 "lost" "1" signal. So remanenz via VR in a LOGO! 8.4 should work as long as no other device activilly change the state of VR0.0. AttachmentVR0_0 Test.zip (438 Downloads) |
Last edited by: AutoGen_380038 at: 08/13/2024 05:36:56 |
|
Follow us on