6/26/2009 2:23 PM | |
Posts: 691 Rating:
|
Yes It worked Set the Q-bit in the end of OB1 is working fine But I can't find QB0,QD0 or Q0.0 written anywhre |
6/26/2009 2:33 PM | |
Posts: 293 Rating:
|
Could you explain it, please? |
6/26/2009 2:45 PM | |
Joined: 10/7/2005 Last visit: 9/3/2025 Posts: 3049 Rating:
|
Hello Rene_10r have a look at this thread concerning ENO and its meaning. Hello Ninja Robot That's good, we are getting somewhere and there is a good chance that indirect addressing is used somewhere after the call of your FB which overwrites the Q 0.6. Owing to the nature of indirect addressing, you won't find this via the X-ref, but you can yourself narrow it down by adding "A Q 0.6"in different places between the call of your FB and the end of OB1 and then check via block status when Q 0.6changes to 0. As mentioned earlier posting your S7 project here won't hurt. cheers fritz |
Last edited by: fritz at: 6/26/2009 2:48 PMCheers |
|
Follow us on