8/27/2024 9:33 PM | |
Joined: 11/24/2018 Last visit: 9/30/2024 Posts: 29 Rating:
|
Hello Experts, I trust you're well. I have a similar problem with the SD card backup. Our original SD card was sent away along with the defective screen for repair (by mistake). The exchange screen provided, had a SD card with a different project on it, which was of no use to us. We have a backup of our original project (.brf) on a USB stick (64G). Is it possible to run it from there without the SD card at all? I have tried a few things but didn't succeed. Is this SD card a special Siemens device? Can our backup (.brf) be copied onto such a SD card and then used? Any help would be very appreciated. Many thanks. Regards, DBME ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/28/2024 08:52:31New subject after splitting |
|
8/28/2024 2:09 PM | |
Joined: 7/11/2024 Last visit: 8/4/2025 Posts: 200 Rating:
|
Hi DBME As itafusna said we need to know which panel are you using in order to help you. Anyway, if it is the same HMI , you should consider performing a restore as it is described here: Backup/restore options for SIMATIC HMI Panels Hope it helps |
If this post has been useful, don't forget to rate it!😊 |
|
Follow us on