(0)| 9/13/2024 1:43 PM | |
|
Joined: 5/31/2024 Last visit: 11/10/2025 Posts: 4 Rating:
|
Hello, I am having problems when activating V90 PN servo drivers with s7 1200 plc. PLC: S7 1215C CD/DC/DC 6ES7 215-1AG40-0XB0 V90 PN Driver: SL3210-5FE13-5UF0 3.5KW 380V Before this, I used Keba, Kuhnke, Sew, Delta, Omron servo motors. This is the first time I am using a Siemens servo motor with a V90 driver.I searched the topics in the forum but could not find a solution. I downloaded a sample project from the site and I am progressing through that project.My network name and IP addresses are OK, I have configured them correctly. When I am online, all my communications are OK. I showed it in the attachments. I also added my configuration and technology object settings to the attachments. I structured them based on sample projects and forums and videos I researched on the internet.Everything looks the same according to the sample project and the information and documentation on the internet., The problems I have are as follows; - When I enable the axis in tia portal axis commissioning, some axes are not enabled. Similarly, when I turn servo on in v-assistant, the axis is not enabled. - When I want to move the enabled axes in v-assistant, it shows that the motor is drawing current, but the motor does not move. There is no heavy load connected to the motor, it can be easily turned by hand. The same thing happens when I separate the motor from the load. - A different motor gives the f31130 error after turning a little. I checked my encoder and power cables. I tried by changing the phase order. I tried by resetting the drivers to factory settings. I tried with two different v90 versions. The results did not change in either. I expect help from relevant and knowledgeable people, can you please help me? As I said, I am new to Siemens servos. AttachmentCilt1.pdf (971 Downloads) |
Follow us on