(0)| 10/8/2024 1:59 PM | |
|
Joined: 3/27/2008 Last visit: 12/30/2025 Posts: 1235 Rating:
|
Have a look here: SINAMICS G120 (CU2x0x-2): Extended functions of motorized potentiometer (MOP) 'Motor Potentiometer' Is a term used by Siemens, using two digital inputs to set a speed: A contact closure at a digital input can increase the speed, open the input and the increasing speed stops or is held at that point. The second digital input when closed will decrease the speed or frequency, and hold that frequency when opened. Parameters: P1030, configuration of the MOP ( Motor Potentiometer). Saving the setpoint, configure the ramp etc. P1035, signal source for 'increase speed'. P1036, signal source for 'decrease speed'. P1037, Maximum setpoint P1038, Minimum setpoint. Tractor |
Last edited by: Moderator_Lan at: 10/08/2024 14:04:11link optimized Tractor |
|
| 10/8/2024 4:30 PM | |
|
Joined: 7/29/2024 Last visit: 10/15/2024 Posts: 6 Rating:
|
була подана команда «старт», але відповіді немає |
Follow us on