10/23/2024 8:52 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello Dezmond13 Which WinCC Version do you use (with SP and Upd)? Which PLC do you use? (seems like some s71200??) Check this FAQ: (Its the same in WiCC V7/8 and WinCC Prof) https://support.industry.siemens.com/cs/de/en/view/98699910 do you use some kind of Hot Standby (like running two independent WinCC Stations) or do you use WinCC redundancy? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on