10/29/2024 8:18 AM | |
Joined: 8/3/2009 Last visit: 9/10/2025 Posts: 16372 Rating:
|
Hello gcanoVFA I think you need the opposite of the parent operator. This is also very easy, it is explained in the Help system: https://support.industry.siemens.com/cs/ww/en/view/109792622/56267519627 Check the VBS example VBS199 in the manual. With this knowlede you can go downwards with the parent operator and then go upwards into the screen windows to dynamise your Trend View control Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
11/5/2024 3:47 PM | |
Joined: 10/30/2022 Last visit: 6/2/2025 Posts: 3 Rating:
|
Thanks Murof! I just had to add the command "Screen" before "ScreenItems" to make it work. Best regards. |
Follow us on