11/7/2024 12:50 PM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi Benny.G, In this case, have you checked that the alarm files are being generated correctly on the USB that you have configured the logs? Maybe they are not being generated and that is why they are not being displayed. It also occurs to me that you might have some filter set in the alarm viewer and that it is discriminating the ones that are archived. Finally, I recommend you to review the TIA Portal V15.1 manual below so you can take a look at the archiving and how to display the alarms in case you have missed something: Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on