(0)| 11/20/2024 5:07 AM | |
|
Joined: 11/18/2024 Last visit: 11/27/2024 Posts: 4 Rating:
|
Dear All, I am using a Siemens Masterdrives model 6SE7021-OEP60 having terminal connectors X101,X102. Currently I am using X101: 9,10 for analogue input 0~10VDC for setpoint and starting command on X101:1 and X102:19. Now I want to use second analogue input 4~20mA in X102: 17,18. So when Digital input 1 is high at X101: 1,3 the 4~20mA signal is followed and when the Digital input at X102:9 is high the analogue input 0~10V is followed. How can I change the parameters to follow this logic. Attached is the current parameter file. AttachmentMASTERDRIVE 9154 Org.zip (319 Downloads) |
Follow us on