12/4/2024 7:31 AM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi AutoGen_5902644, In this case, I am afraid that there is no way to convert a project from WinCC Comfort to WinCC Professional as these are two completely different products with different functionality. You have to recreate the project for the SCADA. Best regards! PD: I forget that to say that you can copy and paste some object but you can't click 'replace device' and let it adapt itself |
Last edited by: ElonksuM_SN_BN at: 12/04/2024 07:33:00Last edited by: ElonksuM_SN_BN at: 12/04/2024 07:54:32If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on