10/23/2024 6:29 AM | |
Joined: 1/2/2014 Last visit: 8/25/2025 Posts: 160 Rating:
|
Hello Friend
I am facing same issue, did you find a solution? Folder exists but no gsd. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/23/2024 07:46:34New subject after splitting |
|
10/23/2024 8:44 AM | |
Joined: 2/17/2020 Last visit: 8/29/2025 Posts: 1251 Rating:
|
Hi, The SIMATIC CPU S7-410-5H Process Automation, proven for many years in the SIMATIC PCS 7 process control system, is now also approved for selected STEP 7 applications. For use in STEP 7 as of version V5.6, however, an additional download of HSP267 V2.0 is necessary. For detailed differences when using the CPU 410 in STEP 7, please refer to the manual below: STEP 7 Operation of CPU 410 in the context of SIMATIC STEP 7 For example, I believe that classic PCS 7 functionalities (such as the expansion of the SEC in RUN or the TCiR function) are not available in operation with STEP 7. |
A rating will be well appreciated. |
|
12/31/2024 7:36 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
https://support.industry.siemens.com/forum/bg/en/posts/looking-for-hsp-267-v2-0/269630 |
Follow us on