1/13/2025 3:47 PM | |
Joined: 10/16/2020 Last visit: 8/27/2025 Posts: 146 Rating:
|
Hello! Verify the properties of the transition in the BATCH Recipe Editor. Ensure that the step enabling conditions are correctly set up with valid operands and logical operators. The conditions should be specified as Boolean expressions and correctly linked to the process tags: SIMATIC PCS 7 process control system SIMATIC BATCH V9.1 SP2 (page605). BR |
Last edited by: Moderator_Lan at: 01/14/2025 07:24:02link optimized If this information has been helpful to you, please don't forget to rate it. |
|
Follow us on