1/14/2025 6:29 AM | |
Joined: 9/10/2024 Last visit: 2/7/2025 Posts: 3 Rating:
|
HI, I have a similar problem right now. I can easily connect with the device using TRCV_C, I can also send data with TSEND_C and it's all good. But the problem is, I'm not receiving two first Chars, they are replaced with '?' and '$R', while monitoring I can see that for a very short time the Chars are correct but in a blink of an eye they are replaced. When not using ad-hoc mode it's working correct but I am receiving data with dynamic data length so I have to use it. Any ideas why is that happening? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 01/14/2025 07:55:03New subject after splitting |
|
Follow us on