6/4/2020 12:05 PM | |
Posts: 11 Rating:
|
Anyone got any solution on this? I am also facing same issue. I have project from other computer, I have installed PCSV9.0 & WinCC7.4. I have retrieved project on OS machine through ES (which is having Step 7) after successful retrieve, I have selected OS-Right click and Compile. it took a while for completion as project is larger size. whereas at end an error is appeared Compile OS (302:309) An error occurred while creating server data. on other hand i tried to open WinCC project directly on WiCC explorer to use Run-Time. when i activate this project on OS Wincc explorer I can see entire graphics as disabled. I can see heading but not allowed to clicked anywhere. In both way I am unable to access HMI. anyone to help on these problems?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/05/2020 10:59:47New subject after splitting |
|
1/22/2025 10:11 PM | |
Joined: 3/21/2015 Last visit: 8/22/2025 Posts: 60 Rating:
|
Hello, Did anyone found a solution for this issue? thank you. Nick. |
Follow us on