(0)| 2/5/2025 6:55 AM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi, Which text do you want to change? You have several options: Set OS additional text for In01, In01.Value and a identifier for AV01. Please bear mark that filling OS additional text for In01.Value does not work->you need to use In01 Also note that when AV01 and In01 are filled in, only the text of In01 is shown. |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 2/5/2025 10:26 AM | |
|
Joined: 8/8/2022 Last visit: 7/14/2025 Posts: 2 Rating:
|
Thank you both. OS full download was helpfull. For: Oreca. I changed the identifier on the I/Os tab of the Interlock. |
Follow us on