4/21/2022 11:19 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi Rui_t, S7-1500 has an integrated system diagostic. There´s an application sample about it, that shows how it works: System Diagnostics with S7-1500 and TIA Portalhope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to
1 thankful Users |
4/26/2022 12:04 PM | |
Joined: 3/25/2015 Last visit: 3/18/2025 Posts: 50 Rating:
|
Hello mopS04, Thank you for the help. I have been studying a bit more and I checked the link you sent. This is perfect and kinda what i´m looking for but the problem is I need this information to integrate into a WPF based scada system. Everything I´ve seen is internal between Siemens components. For example the system diagnostic view component in TIA panels brings a list of everything that is configured in the hardware and with S300/S400 CPUs I was able to get the complete network information with just a few lines of code with SFC51, not having to worry about diagnostic addresses or how many nodes are configured. this is all given automatically by sfc51. This is what I am trying to achieve also with 1500 CPUs. A simple and efficient why to retrieve the network information without having to call "ModuleStates" and "DeviceStates" for every node. |
10/24/2024 8:04 AM | |
Joined: 2/27/2024 Last visit: 8/16/2025 Posts: 17 Rating:
|
Thank you |
2/11/2025 10:16 AM | |
Joined: 1/16/2020 Last visit: 9/9/2025 Posts: 1 Rating:
|
thank you |
Follow us on