(0)| 2/13/2025 10:47 PM | |||||
|
Joined: 4/11/2022 Last visit: 12/30/2025 Posts: 95 Rating:
|
Find attached my example for you. Explanation what I did... Firstly you do need to declare variables to be used. Go to "Tools" -> "Parameter VM Mapping..."
Think that 2 hours and 40 minutes is a total of 160 minutes. In my program you can simulate, open Data Table -> in VW0 write 160 and in VW2 write 160 as well. DONE! You can see that the total time will be 160 min = 2 hours + 40 minutes. You can change also the time base. Declare as follows in "Tools" -> "Parameter VM Mapping...":
If you write in VB4 number 3 means (h:m) If you write in VB4 number 2 means (m:s) If you write in VB4 number 1 means (s:ms) *********************************************************************************** To be honest, in separate way as you desired I did not reach. *********************************************************************************** Hope it helps. AttachmentTest_Navid_Neshat56.zip (190 Downloads) |
||||
Last edited by: PADRE PIO at: 02/13/2025 23:00:40Last edited by: PADRE PIO at: 02/14/2025 00:03:47Rgds, |
|||||
Follow us on