1/19/2025 8:08 PM | |
Joined: 1/19/2025 Last visit: 2/23/2025 Posts: 1 Rating:
|
Dear all , Hello every one I am working on a project to control a Festo ServoPresse KIT "YJKP," which consists of a driver "CMMT-AS-C12-11A-P3-MP-S1" and a Festo PLC "CECC-X-M1." I can control the driver using the Festo Automation Suite application and have made modifications to the network and communication protocols. I established a Profinet connection between the Siemens PLC "6ES7 214-1HG40-0XB0" and the Festo driver (as shown in the attached pictures). However, when I attempt to control it using the FBD "Festo_PtP_Drives_PN," I encounter an error code that alternates between "8401" and "8402." Despite I follow the correspending pdf file for the inputs configurations So my questions are :
Thank so much AttachmentCMMT ISSUE.docx (156 Downloads) |
Haythem Miraoui |
|
Follow us on