8/10/2017 12:42 PM | |
Joined: 12/21/2009 Last visit: 8/8/2025 Posts: 39 Rating:
|
Hi, I have similar question: Is this allowed and safe tu run PROFINET and MODBUS TCP in the same network or it will cause some problems in the network (conflicts, higher network load)?. Here is the situation I have: I use CPU 3172-PN/DP. On integrated port I run my PROFINET network (several frequency converters, ET200S, AS-I masters, etc...) Now to this network I want to add device that can only communicate using MODBUS TCP. I investigated that I could use "S7 OPEN MODBUS / TCP Communication via the integrated PN interface of the PLC" (https://w3.siemens.com/mcms/topics/en/siplus/ric-telecontrol/Documents/ric-docu/modbus-tcp_funktionsbeschreibung_en.pdf) Will this mix be safe for my PROFINET devices? Regards, Piotr------------------------------------------------------------------------------------------ |
Last edited by: azi1984 at: 8/10/2017 12:43:51 PMLast edited by: Jen_Moderator at: 8/11/2017 11:08:29 AMNew subject after splitting |
|
8/10/2017 2:09 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, yes it is allowed and safe. You find this question very often here in the forum. see this one: PROFINET TCP/IP and Modbus TCP/IP hope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to
2 thankful Users |
Follow us on