2/27/2025 1:52 PM | |
Joined: 2/1/2010 Last visit: 9/5/2025 Posts: 212 Rating:
|
The picture tree for the webclients is based on the picture tree of the station which you are running webnavigator on. Make sure you publish the webserver 2x - once for the server data, and once for the 'client data' - aka the picture tree, if these are different. Typically in our architectures we have OS1, OS2, WS, OC1...OCn, with WS being a client OS project machine dedicated to running the WS runtime. on the WS you publish the OS server to get the main pictures (server prefix publish), then publish itself for the navigation, faceplates, picture tree, etc. You need to select the specific graphics applicable for each publish when doing this and not overlap them. |
If my post helped you, please rate. Thanks. |
|
Follow us on