3/26/2025 6:18 AM | |
Joined: 7/26/2022 Last visit: 4/25/2025 Posts: 12 Rating:
|
Hello I Couldn't download it , it shows this: The desired entry could not be found. You are not authorized to access the entry. I need to download software update(SP1) for PCS 7 V8.2 |
3/26/2025 11:54 AM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
Hi, The user should update the links because the PCS7 V8.2 is now a legacy product which means you need a LSS contract in order to get support for older versions. For now only as of V9.1 is still supported |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on