(0)| 2/19/2025 12:51 PM | |
|
Joined: 2/19/2025 Last visit: 4/8/2025 Posts: 4 Rating:
|
Hello, I apologize for the inconvenience, I need help with the following: I have a cnc with a sinumerik 810d, pcu20 controller I need to send programs via ethernet, I have already done all the network configuration part, and I can access the program on the machine via ethernet, but I always have to copy the program from my "Ncdata" folder to the "Part progrms" folder, this becomes very difficult in very large programs, I wanted to know if it is not possible to run the program directly from the folder, without having to copy AttachmentEXAMPLE 2.zip (204 Downloads) |
Last edited by: Moderator_Lan at: 02/19/2025 15:41:55Title updated / text formatting optimized |
|
| 4/7/2025 7:44 AM | |
|
Joined: 2/19/2025 Last visit: 4/8/2025 Posts: 4 Rating:
|
Hi, yes i solved the problem wit your pdf, thaks |
Follow us on