(0)| 4/17/2025 7:26 PM | |
|
Joined: 4/17/2025 Last visit: 4/17/2025 Posts: 1 Rating:
|
Hi, I'm currently working on a very similar project, which I'm in the process of estimating. To avoid creating a duplicate thread, I decided to join this one. In my application, besides an identical Racetrack setup, I’m planning to use an additional 3–4 servo drives for simple tasks such as controlling a box conveyor, product pusher, etc. In total, I expect to use up to 6 servo drives, including two dedicated to Racetrack synchronization. Is a technology version of the CPU necessary for such an application? I'm considering either the 6ES7511-1FL03-0AB0 or the 6ES7511-1UL03-0AB0. Which drive system would be the most suitable? I was looking into the SINAMICS V90, but the SINAMICS S210 series also caught my attention. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 04/22/2025 06:20:58New subject after splitting |
|
Follow us on