(0)| 12/7/2022 1:59 PM | |
|
Joined: 12/23/2016 Last visit: 3/20/2025 Posts: 4 Rating:
|
Hello everyone, AttachmentSIA_WINCC_COMFORT_V14_SP1_Upd10.txt (444 Downloads) |
| 12/7/2022 2:02 PM | |
|
Joined: 5/12/2006 Last visit: 12/19/2025 Posts: 22816 Rating:
|
wrong logfile in the attachment |
| 12/7/2022 2:15 PM | |
|
Joined: 12/23/2016 Last visit: 3/20/2025 Posts: 4 Rating:
|
Sorry, which file I should send? |
| 12/7/2022 2:23 PM | |
|
Joined: 12/23/2016 Last visit: 3/20/2025 Posts: 4 Rating:
|
should be this one;AttachmentSIA_WINCC_COMFORT_V14_SP1_Upd10@22-12-07_12-08-44.zip (489 Downloads) |
| 4/30/2025 9:48 AM | |
|
Joined: 7/10/2024 Last visit: 12/23/2025 Posts: 180 Rating:
|
Hello AndreaM. Unfortunately, I couldn't find anything clear in the log. But in case it helps you, I share with you how to make the installation as clean as possible to try to reduce failures as much as possible - Clean reboot -> How to perform a clean boot in Windows - If it is compressed, unzip it to the shortest possible path within the hard drive. If not, also use a short path avoiding special characters - Run as an administrator |
|
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
| 5/6/2025 7:58 AM | |
|
Joined: 8/3/2009 Last visit: 12/19/2025 Posts: 16612 Rating:
|
Hello AndreaM. do you use the download of the V14 SP1 Upd10 image from this website : https://support.industry.siemens.com/cs/de/en/view/109746074 or do you use a installation iso/dvd with only v14 SP1? and also if you have installed Step7 Prof V14 Sp1 first with which installation files do you inistall ist? you should use both inistallation iso from the link above (Step7 and WinCC comfort/advanced) Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on