(0)| 5/6/2025 12:30 PM | |
|
Joined: 1/18/2025 Last visit: 5/7/2025 Posts: 1 Rating:
|
facing an issue in my project using AI v1.0.1 and AQ v1.1.3 but this firmware version not available in my tia portal software(v18) . i have downloaded v18 hsp files after also cant change firmware version my configuration is s7-1500 with et200sp im getting error msg A hardware component is or was inserted, but an error has occurred during module parameter assignment. Possible causes: The hardware component is faulty. The product version of the hardware component does not match the version for which the configuration was created. Resolution: Replace the hardware component. Check the product version of the hardware component and insert a suitable version of the module, if necessary. Remove and reinsert the hardware component. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 05/06/2025 14:37:49New subject after splitting |
|
Follow us on