(0)| 1/17/2023 10:47 AM | |
|
Joined: 1/21/2013 Last visit: 12/29/2025 Posts: 4367 Rating:
|
Hi Juha121212, to retrieve data via ENTSO-E the LHTTP library could be the right way. In fact, it is the only library from Siemens that I know of that could do this. Providing more information on your issue will help us. Kind regards |
| 1/18/2023 10:22 AM | |
|
Joined: 1/21/2013 Last visit: 12/29/2025 Posts: 4367 Rating:
|
Hi Juha121212, status code 16#7002 is not an error, i.e. the command is executed. An error is indicated if the most significant bit is set to TRUE, i.e. for codes 16#8xxx. Your error code 16#8601 means Error in subordinate command "TSEND_C" (see chapter 4.8 of the documentation provided with the Libraries for Communication for SIMATIC Controllers). To investigate further, look in "diagnostics.subfunctionStatus" and find the code given in the table "ERROR and STATUS parameters" in the description of "TSEND_C". Kind regards |
| 5/12/2025 12:46 PM | |
|
Joined: 12/19/2018 Last visit: 12/2/2025 Posts: 1 Rating:
|
Hi. Anything new about ENTSO e data on Simatic? Best regards. |
Follow us on