(0)| 5/18/2025 7:11 PM | |
|
Joined: 3/11/2025 Last visit: 6/18/2025 Posts: 1 Rating:
|
I have some issues with allowing anonymous access to SIMATIC NET OPCUA server. The first guide on the topic Data Exchange between S7 Station and PC Station with SIMATIC NET OPC Server I have a Windows server with SIMATIC NET v20 running a OPC-UA server that are connected to Siemens 1517H plc's over S7 protocol. I am aware the plc's have built in OPC, but the client requires a stand alone solution. The anonymous login is enabled on the server.(picture1) When i connect to the server with UAExpert, i can connect as anonym.(picture2) I can even get overview of the data structure.(picture3) The issue comes when im dragging the tags over to the data access view. Nothing is happening except error in the log.(picture4) If i change to log in with username and password, everything works as it should. i am logging in with the Windows username and password.(picture5) I have tried looking into windows access restrictions, but i cant find anything in the documents. Is there anything i have to change in the config files of the server? K Attachmentpictures2.docx (123 Downloads) |
Last edited by: Moderator_Lan at: 05/19/2025 06:53:29link optimized |
|
Follow us on