2/16/2024 1:58 PM | |
Joined: 7/19/2022 Last visit: 9/2/2025 Posts: 436 Rating:
|
Hello Kristof74, I had the same problem with TIA Portal V17 and following the following steps solved it: 1. Deinstall V18 completely 2. Download the DVD with TIA V18 Setup 3. Store the DVD locally 4. Install TIA Portal as Admin, deactivate the antivirus-programs during the installation. 5. Try again if it is possible to install GSD files. Also check that there is compatibility between your software and your OS: Compatibility Tool |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
2 thankful Users |
4/5/2024 2:00 PM | |
Joined: 10/23/2023 Last visit: 4/17/2025 Posts: 3 Rating:
|
How did the compatibility tool help you? Also, did you have to uninstall V18 completely? |
4/17/2024 11:57 AM | |
Joined: 7/28/2022 Last visit: 10/29/2024 Posts: 9 Rating:
|
I didn't have to uninstall TIA portal. I had an incompatible STARTDRIVE version with my TIA Portal version. --- Kristof |
5/27/2025 11:34 AM | |
Joined: 3/21/2025 Last visit: 5/27/2025 Posts: 1 Rating:
|
Same Problem here. What did you do? Uninstall Startdrive? |
Follow us on