6/24/2025 8:00 AM | |
Joined: 1/27/2025 Last visit: 6/24/2025 Posts: 12 Rating:
|
Hello! This is my first try to develop a SCADA system in WinCC Unified PC. I am using S7 1214C CPU with firmware version 4.6, Unified PC and TIA portal V19 for my project. I am going to use same PC as engineering PC and Server PC. I have created Root Certificates and tried to connect with the PLC. I have followed the below link to do that. https://support.industry.siemens.com/cs/bo/en/view/109806850 But still it says that "Timeout while establishing the connection to @6%s@" in my alarm page. What is the possible reason for this? |
Last edited by: Moderator_Lan at: 06/24/2025 08:47:01Images embedded from link / Link optimized |
|
6/26/2025 1:10 PM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello AutoGen_4865062 Check also the security settings : https://support.industry.siemens.com/cs/de/en/view/109955142 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on