7/3/2025 11:29 AM | |
Joined: 8/3/2009 Last visit: 9/19/2025 Posts: 16461 Rating:
|
Hello Tech Ahmed to use the OPC UA Server of the WInCC Rutnime you have to install it (from main installation dialog)and you would need a Connectivity pack license that it works. If you only want to use the OPC UA Client channel in WinCC this will not need an additional license. How to set up both is described well in the manual: https://support.industry.siemens.com/cs/ww/en/view/109987033/189197927691 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on