(0)| 7/17/2025 3:42 AM | |
|
Joined: 12/18/2014 Last visit: 1/11/2026 Posts: 36435 Rating:
|
TM FAST - Supplementary Software Components for STEP 7 (TIA Portal) and Intel Quartus Prime Software Update 07/25The TM FAST technology module offers extremely fast processing in the S7-1500/ET 200MP system. The TM FAST function can be programmed by the user and allows internal cycle times of up to 20 nanoseconds. ere you will find additional software components, some of which are required to operate the TM FAST or make it easier to use. The user-programmable technology module S7-1500 TM FAST offers the user the option of programming the function of the module for specific applications. For this purpose, an application is created using the Intel® Quartus® Prime engineering tool chain from Intel and loaded into the TM FAST. There, the program is processed in an FPGA (Field Programmable Gate Array). The user has direct access to the digital inputs and outputs. In this entry you will find a series of SW components for the development and operation of TM FAST. |
This contribution was helpful to
|
|
Follow us on