(0)| 8/7/2025 3:25 PM | |
|
Joined: 6/7/2022 Last visit: 12/23/2025 Posts: 9 Rating:
|
WinCC V7.5 + SP2 + Upd9 The Alarm type selection button banner, ButtonsC.PDL, disappeared on the alarm page in WinCC run time. This is the button banner that allows you to switch between new, old, gone, active, journal, hidden, etc alarm pages. Looks like it fails on the Creates / updates the structure tag '@Diag_*_Overview' The help on that says to go into Tag Management and blow those tags away so the system can recreate them but they are protected read only and you can't delete them. Looking for a solution that will get my alarm banner back and fix this internal configure error. Thanks! AttachmentAlarm and OS Editor Errors.pdf (643 Downloads) |
Last edited by: BigRedBeard at: 08/07/2025 15:31:30Last edited by: BigRedBeard at: 08/07/2025 15:44:51 |
|
Follow us on