(0)| 8/17/2025 9:40 AM | |
|
Joined: 6/11/2019 Last visit: 12/31/2025 Posts: 2712 Rating:
|
Zip this file and upload it. Regards, Ella_68 |
| 8/17/2025 10:35 AM | |
|
Joined: 7/14/2024 Last visit: 8/25/2025 Posts: 7 Rating:
|
AttachmentBewaring cellen 2025.zip (99 Downloads) |
| 8/17/2025 11:14 AM | |
|
Joined: 12/18/2014 Last visit: 1/1/2026 Posts: 36393 Rating:
|
There's a problem with LSC V8.3.x and LSC V8.4.x. I can load the diagrams without problems with LSC V8.0, V8.1.1 and LSC V8.2.x. No password request. I can't help you. Start a Support Request and ask Siemens directly if they can help you. |
| 8/17/2025 11:59 AM | |
|
Joined: 6/11/2019 Last visit: 12/31/2025 Posts: 2712 Rating:
|
Hello bart_res145, Fortunately, the individual LSC files aren't encrypted. I extracted them from the network project. Now you just need to import them into a new network project and complete the network again. It's a bit of work, but better than rewriting everything. Regards, Ella_68 (translated by Google) By the way, starting with LSC 8.3.0, there are problems loading programs from older versions.Since you upgraded from LSC 8.2.1 to 4.0, the older version should still be there as a base.Use it for the older programs. AttachmentLogo8 Cel.zip (104 Downloads) |
Last edited by: Ella_68 at: 08/17/2025 13:16:26new Program |
|
Follow us on