(0)| 8/25/2025 10:00 AM | |
|
Joined: 7/22/2025 Last visit: 12/25/2025 Posts: 40 Rating:
|
yes, this is the solution, thanks a lot sir! i need another tip from you, i have an analog pressure sensor from -1 to 10 bar and i want to view it as floating-point value as it shows -0.4 bar as 0 bar and -0.6 bar as -1 bar, is it doable to view floating-point in logo! thanks in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/25/2025 11:16:15New subject after splitting |
|
| 8/25/2025 10:49 AM | |
|
Joined: 7/22/2025 Last visit: 12/25/2025 Posts: 40 Rating:
|
yes, i had to add the tag scaled by *10 and then add them to web editor with 1 decimal place! thanks |
Follow us on