(1)| 7/27/2009 1:08 PM | |
|
Joined: 9/27/2006 Last visit: 12/29/2025 Posts: 12477 Rating:
|
Hello duy; The BETA line of multimeters (of which your multimeter model is a part of)seems to be associated with the Siemens Building Technologies division: There are different manuals on BETA multimeters there, inclding your model. For information on communications for your multimeter model, start by doing a search in the download section of the SBT support pages, on Modbus or LAN coupler for example: http://www.buildingtechnologies.siemens.com/bt/global/en/support/Pages/download.aspx It looks like the application for the LAN coupler is dedicated to PC connections. You could possibly try the option of Modbus RTU with the PLC, or even Modbus/TCP. The multimeters also offer a pulse output that you could read as a counter value. |
Follow us on