(0)| 8/25/2009 12:23 PM | ||
|
Posts: 9 Rating:
|
Hi Peter, This my board is measuring NTC resistors and any resistorsand gives the result as pulses, which is counted by Logo digital input. Normal Logo input can count only 4 Hz speed. Fast input can count 5kHz speed. Output of my board can be set by hardwareresistor and capacitor on board. Calculation formula is t1 = 0,693(R1+R2+R3)*C t2 = 0,693 (R3*C) t2 is fixed to 125ms (4Hz) and t1 is changing. Speed can be set high, if you use fast input of Logo. More info, contact matti.niemi@fi.abb.com |
|
Follow us on