(0)| 12/4/2009 6:20 PM | |
|
Posts: 32 Rating:
|
Hello Lifrasil, Helmut_13, Betel and expert, I'm new user for LOGO! . I just create sample circuit " DOL Starter " in LD. Once i convert to FB, the question are ; i.) Why block number not have B003 ???Same time i upload my circuit for expert to clarify. I look forward to a favourable reply from you. Thank for expert. regard, Nelson. AttachmentCopy of DOL Starter1.zip (564 Downloads) |
Last edited by: liew at: 12/5/2009 5:45 AM |
|
| 12/6/2009 7:10 PM | |
|
Joined: 3/4/2009 Last visit: 10/28/2020 Posts: 57 Rating:
|
Ηι. Your program demands to connect a button with a normaly open contact (the stop button) to I2 of logo. That's not a good practice. You should use a "make contact", and connect a button with a normaly closed contact at I1. In order to help you understand fbd, I changed a little the result of the convertion that logo made. The logic is exatly the same. I just used a "NOT" function instead of reverting the inputs of the "AND" functions. Inverted inputs are represented with a dot. You can invert an input of a function by a doubleclik on the input. Do you understand the program i uploaded? AttachmentDOL Starter fbd.zip (592 Downloads) |
This contribution was helpful to
|
|
Follow us on