(0)| 8/1/2006 9:20 AM | |
|
Joined: 4/24/2006 Last visit: 12/24/2025 Posts: 9097 Rating:
|
Hello abproj, It looks that it's a compatibility problem. http://support.automation.siemens.com/WW/view/en/22056585 You should upgrade your Step7 software. Best regards, Wizard |
| 8/5/2006 12:42 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="abproj"]I have had Step7 V5.2 SP1 on my laptop (Win2000 SP4) for about 2 years. About a month ago I opened a big PLC program that was generated in Step7 V4 and ran Reorganize from Simatic Manager. I also installed WinCC Flexible 2005 and got the new Automation Licence Manager. Hi Abproj, There is also a hotfix 3 (contains also HF1 and HF2) for STEP7 V5.2 SP1, maybe that brings some difference: STEP 7 V5.2 SP1 + Hotfix 3 Now Available I don't think that that solve your problems, but not shooting is always miss... [:o] If you want that I look in STEP7 V5.4, whats happening, then please place the project (max.1MB) to the Forum. When it is bigger, please send me a Private Message with your Email-Address and I will give you my email-address so that you can send the Projekt to me (max. 5MB). [;)] When it could be opened by V5.4 then a Upgrade of the software is the best, also because WinCC Flexible 2005 (SP1 can now also be downloaded) is working with S7 V5.4 the best.[:blush:] |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on