(0)| 2/8/2010 2:52 PM | |
|
Joined: 9/23/2005 Last visit: 12/29/2025 Posts: 4435 Rating:
|
Hi, you can use 5x the Norm to convert each one of your 5 analogic values to normalized values. After that for each one you can use a Scale to rearrange the scale. you can also mount a FC with this two blocks (like the TIP /tf/WW/en/Posts/31698#top) and call it 5 x. The address number indicate the first byte of the variable. A word uses two bytes. So, IW0 uses byte 0 and 1. The next IW is IW2 (bytes 2 and 3). |
Last edited by: Pegaia at: 2/8/2010 2:53 PMDenilson Pegaia |
|
Follow us on